ARD2  1.00 for Rev B. Hardware
Airbag Reference Demonstrator using MPC5604P
eTIMER.c File Reference

This file is empty. More...

#include "Compile_Options.h"
#include "derivative.h"
#include "ETIMER.h"

Functions

uint8_t u8SampleFn (const uint16_t *pu16RawResponse, uint8_t *pu8Response, uint8_t u8Size)

Detailed Description

This file is empty.

Copyright (c) 2011 Freescale Semiconductor Freescale Confidential Proprietary

Author:
Freescale Semiconductor
SASD Automotive
Author's CoreID
Version:
Date:
Warning:
(If needed)

History: